IMX6D: Hardware accelerator not working on "chromium-ozone-wayland"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D: Hardware accelerator not working on "chromium-ozone-wayland"

797 Views
david5icp
Contributor III

Hi,

We have compiled with "DISTRO=fsl-imx-xwayland MACHINE=imx6qsabresd", the image "imx-image-multimedia" and chromium-ozone-wayland with yocto Zeus. The benchmark is very low on chromium.

We check the GPU setting of chromium as below:

Table 1.

Graphics Feature Status
Canvas: Hardware accelerated
Flash: Hardware accelerated
Flash Stage3D: Hardware accelerated
Flash Stage3D Baseline profile: Hardware accelerated
Compositing: Hardware accelerated
Multiple Raster Threads:  Force enabled
Out-of-process Rasterization: Hardware accelerated
OpenGL: Enabled
Rasterization: Hardware accelerated
Skia Renderer: Enabled
Video Decode: Hardware accelerated
Vulkan: Disabled
WebGL:  Hardware accelerated
WebGL2:  Hardware accelerated

(the settings above are applied to both Zeus & Krogoth)

The benchmark compare with krogoth for reference:

Table 2.

NXP BSP releaseZeusKrogoth
Yocto version3.02.1
Linux kernel version5.4.704.1.15
Chromium version8348
FPS ~52 ~56
Bunnies12003100

 

We discover that there is a patch for version 48 which links shown below from NXP, but there is no much difference after remove this patch.

https://github.com/Freescale/chromium-imx

According to Table 1, most features (except Vulkan) are enabled and accelerated, but it seems hardware acceleration feature does NOT really activated.

therefore, please help to guide us to activate hardware accelerator for Chromium Browser.

0 Kudos
Reply
0 Replies