Hello,
We are developing a custom hardware solution with the SJA1105TEL which connects a PHY, SBC and a FPGA with RGMII interface. Is there a default configuration provided by NXP that we can upload using the sja1105-tool to get the system running with basic functionality like forwarding packets from the PHY to the SBC ?
Kind Regards
Arun.
Hi Platon,
I have found the Python file you were referring to: /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py.
I found out that the following parameters depend on the board layout, so they need to be changed for my application:
Is there any other board-specific (e.g. port dependent) register I need to change? If I just changed the above two parameters, would it work?
The block diagram of my system is available below. I just want my three devices (i.e. Jetson Xavier AGX, ethernet jack, and the other MAC device) to communicate.
Regards,
Hermawan Mulyono
EDIT: I should have replied to @bpe 's post directly, but I could not post two messages in an hour.
To be clear: there is no one-fits-all configuration for SJA1105 switch. What example_configs/pyScripts/ directory provides, is a set of more-or-less typical configurations for a reference. You can start with the one that is close to what your board needs, but it cannot save you reading the documentation. Refer to AH1601 for board and interface specific parts of the switch configuration.
Best Regards,
Platon
If on your board all switch connections are RGMII, you can start with /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py. Thie file is part of the configuration tool SW package. Details can be found in AH1601
Hope this helps,
Platon