Teensy Prop Shield : Motion activated Light
This demo shows a basic gesture controlled light sequence using NXP motion sensors available in the Teensy Prop Shield
LED lights can be found on the following link: https://www.adafruit.com/product/2238
Features
The Teensy Prop Shield is an add-on sensor shield board for the Teensy 3.1 which is an USB based microcontroller development platform. The Teensy 3.1 has a 32 bit ARM Cortex M4 processor from NXP -MK20DX256. The board can be programmed using Arduino IDE + Teensyduino plugin.
The prop shield consists of the following devices:
Featured NXP products
Demo Setup:
Wiring[1] :

Software:
After setup, Download Arduino IDE and Teensyduino add on and follow the instructions as defined in the page below
http://www.pjrc.com/teensy/td_download.html
Note: Arduino version used for this demo: 1.6.8.
Run the “Teensy_RGB_Led_Strip.ino” sketch attached.
Sample Code:
// Full orientation sensing using NXP's advanced sensor fusion algorithm.
//
// You *must* perform a magnetic calibration before this code will work.
//
// To view this data, use the Arduino Serial Monitor to watch the
// scrolling angles, or run the OrientationVisualiser example in Processing.
#include <NXPMotionSense.h>
#include <Wire.h>
#include <EEPROM.h>
#include <FastLED.h>
#define NUM_LEDS 60
CRGB leds[NUM_LEDS];
NXPMotionSense imu;
NXPSensorFusion filter;
int a;
int acc_rms;
void setup() {
Serial.begin(9600);
imu.begin();
filter.begin(100);
delay(2000);
FastLED.addLeds<APA102,11,13,BGR,DATA_RATE_MHZ(1)>(leds, NUM_LEDS);
pinMode(7, OUTPUT);
digitalWrite(7, HIGH); // enable access to LEDs
}
void loop() {
float ax, ay, az;
float gx, gy, gz;
float mx, my, mz;
float roll, pitch, heading;
if (imu.available()) {
// Read the motion sensors
imu.readMotionSensor(ax, ay, az, gx, gy, gz, mx, my, mz);
// Update the SensorFusion filter
filter.update(gx, gy, gz, ax, ay, az, mx, my, mz);
// print the heading, pitch and roll
roll = filter.getRoll();
pitch = filter.getPitch();
heading = filter.getYaw();
Serial.print("Orientation: ");
Serial.print(heading);
Serial.print(" ");
Serial.print(pitch);
Serial.print(" ");
Serial.println(roll);
a=abs(roll/3);
Serial.print(" ");
acc_rms=sqrt(ax*ax+ay*ay+az*az)/3;
Serial.println(acc_rms);
//flash red if a violent shake event is detected
if(acc_rms==1)
{
for(int n = 0; n < NUM_LEDS; n++)
{
leds[n] = CRGB::Red;
FastLED.show();
delay(8);
leds[n] = CRGB::Black;
}
}
// Move a single white led as per rotation
for(int n = 0; n < NUM_LEDS; n++)
{
if(a==n)
{
leds[n] = CRGB::White;
FastLED.show();
delay(8);
}
else
{
leds[n] = CRGB::Black;
}
}
}
}
Sample Code: