Sub-GHz Wireless Mesh Networks using NXP’s Single Chip Modules

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sub-GHz Wireless Mesh Networks using NXP’s Single Chip Modules

Sub-GHz Wireless Mesh Networks using NXP’s Single Chip Modules

The demo from Code is an ultra-compact Sub-GHz to Wi-Fi Border Router solution for use in Home Automation Wireless Sensor Nodes, Smart Lighting, Smart City, Smart Meters, Smart Parking and IoT. The demo consists of an NXP SCM-i.MX 6SoloX V-Link device (i.MX6SoloX/PF0100/512MB LPDDR2) + Code V-Link Top board with 802.11a/b/g/n/ac module + Code Carrier board with the Phalanx Border Router. The Phalanx Border Router provides an optimized mesh network for sensing applications

SCM V-Link technology is ideal for space-constrained applications allowing customers to integrate vertically.

Features:

  • Top board: Broadcom 2.4 GHz & 5 GHz Wi-Fi, 802.11 a/b/g/n/ac , up to 390 Mbps. U.FL standard antenna connector.
  • SCM-i.MX6 SX V-Link Top board form factor, 15.5mm x 15.5mm.
  • Optimized mesh network for sensing applications. Thousands of nodes, minimizing deployment costs. 900 MHz Wireless. A new, clever routing algorithm which reduces routing overhead.
  • IPv6 capable

__________________________________________________________________________________________________________________

Featured NXP Products:

__________________________________________________________________________________________________________________

149329_149329.jpgpastedImage_14.jpg  149336_149336.jpgpastedImage_15.jpg

ラベル(1)
タグ(2)
添付
コメント

This is great. But is there a similar solution for bridging Thread and Sub-GHz bands?

評価なし
バージョン履歴
最終更新日:
‎05-09-2016 03:28 PM
更新者:
NXP Employee