Brillo OS and Weave application protocol on i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Brillo OS and Weave application protocol on i.MX6UL

Brillo OS and Weave application protocol on i.MX6UL

This demo consists of the Pico 6UL evaluation SOM and Hobbit carrier board from TechNexion running Brillo OS and the Weave application protocol.  An air sensor module from MicroElecronica is attached to the board via the MicroE Clicks expansion header.  The Air Quality sensor module monitors the surrounding environment and an alert is triggered if the quality of the air falls below a predetermined level.  The data is transferred from the board to an external device utilizing the weave protocol that is present on both the Pico6UL and the corresponding android device. The alert is shown via an app on android build on the Weave API.

 

Features:

 

Hardware:

1)      Pico i.MX6UL SOM and Hobbit carrier board from TechNexion

2)      Air Quality Click from Mikore http://www.mikroe.com/click/air-quality/

      3)       An Android based tablet

 

Software:

1)      Brillo OS

2)      Weave application protocol

3)      APK file showing UX based on Weave API

 

_________________________________________________________________________________________________________________

 

Featured Products:

标签 (1)
无评分
版本历史
最后更新:
‎05-04-2016 10:58 PM
更新人: