pn7150 unable to integrate to android pie

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pn7150 unable to integrate to android pie

851 Views
harry2220
Contributor II

Hi,

i am trying to integrate PN7150 NFC module to my android board. I am integrating drivers to Android Pie version by following AN11690, which is officially available. i have followed the steps of integration given AN11690 and build it but unable to enable the functionality of NFC in Settings. Can someone help me doing this needful.

Thanks 

Tags (2)
0 Kudos
2 Replies

721 Views
jimmychan
NXP TechSupport
NXP TechSupport

Is there any error message? what is the software and hardware environment of this case?

0 Kudos

614 Views
alfi_fauzi
Contributor I

Hello Jimmychan

i have same problem.  unable to integrate with android 8.1.0.

i follow this document AN11690.pdf. first it says i need to add repo init. so i add this command ;

repo init -m LINUX/android/.repo/local\_manifest/nxpnfc\_manifest.xml
Downloading Repo source from https://chromium.googlesource.com/external/repo
remote: Counting objects: 265, done
remote: Total 7291 (delta 4910), reused 7291 (delta 4910)
Receiving objects: 100% (7291/7291), 2.65 MiB | 0 bytes/s, done.
Resolving deltas: 100% (4910/4910), done.
fatal: manifest url is required.

here i include my error log.

can you give advice.

Thanks, 

 

0 Kudos