pn7150 unable to integrate to android pie

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pn7150 unable to integrate to android pie

2,124 次查看
harry2220
Contributor II

Hi,

i am trying to integrate PN7150 NFC module to my android board. I am integrating drivers to Android Pie version by following AN11690, which is officially available. i have followed the steps of integration given AN11690 and build it but unable to enable the functionality of NFC in Settings. Can someone help me doing this needful.

Thanks 

标记 (2)
0 项奖励
回复
2 回复数

1,994 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Is there any error message? what is the software and hardware environment of this case?

0 项奖励
回复

1,885 次查看
alfi_fauzi
Contributor I

Hello Jimmychan

i have same problem.  unable to integrate with android 8.1.0.

i follow this document AN11690.pdf. first it says i need to add repo init. so i add this command ;

repo init -m LINUX/android/.repo/local\_manifest/nxpnfc\_manifest.xml
Downloading Repo source from https://chromium.googlesource.com/external/repo
remote: Counting objects: 265, done
remote: Total 7291 (delta 4910), reused 7291 (delta 4910)
Receiving objects: 100% (7291/7291), 2.65 MiB | 0 bytes/s, done.
Resolving deltas: 100% (4910/4910), done.
fatal: manifest url is required.

here i include my error log.

can you give advice.

Thanks, 

 

0 项奖励
回复