I am using the Android App "NFC TagWriter by NXP" (v4.1) to write onto an NTAG213 chip from NXP. All of the write operations fail (format, write data set etc.). The erase operation for example shows "Erase failed" (translated from the German "Löschen Fehlgeschlagen"). There is not additional information about a reason that I can see.
The tags can be written with other hardware (e.g. Andruino with PN532 shield). The tags can also be written by another application running on the Nokia 3. So it appears to be a software problem, not hardware.
The device is a Nokia 3 (TA-1032). It is running Android 7.0, build 00WW_1_39M.
I can confirm this. I also have a Nokia 3 (HMG Global TA-1032), currently using Android 8.0.0 (German settings). NFC works perfectly and I can write my NFC tags as I want. I'm using NFC Form Type 2 / NTAG213. While writing to the tag I just receive an error but no further details.
Using g a different tool to write my tags everything works fine. So I agree, there must be a special problem in the NXP App coz that's the single point of issues.
JJ (northern Germany)