I can't find a demo about write typeA card in libnfc-nci demoAPP(i mean raw exchanges),so i have to code by myself.But when i run the code on my board, it return some data i can't understand:
NFC Tag Found
Type : 'Type A - Mifare Classic'
NFCID1 : 'B9 D9 E8 78 '
NDEF Content : NO, mode=1, tech=8
Mifare Authenticate command sent
Response :
40 00
Mifare Read command sent
Response :
10 00 01 02 03 04 05 06 07 08 09 0A 0B 0C 0D 0E 0F 00
Mifare Write command sent
Response :
10 B2
Mifare Read command sent
Response :
10 04 00
NFC Tag Lost
Waiting for a Tag/Device...
where can i get the mean of the response data? And i sincerely hope that NXP can relase a demo about card write(the tag-raw_example in https://github.com/NXPNFCLinux/linux_libnfc-nci_examples Write function not included).
Hi,
The PN7150 firmware supports the NCI specification. The mean of the response data you can find the NFC Controller Interface (NCI) Technical Specification Version 2.1 in the NFC Forum.
Also, we provide additional extensions bot are proprietary to NXP
Regards,
Mario
Hi,
Please follow the next link.
NFC Controller Interface (NCI) Technical Specification Version 2.1
You need to log in to the NFC Forum
Regards,
Mario