Vdd for Pullup on FDpin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vdd for Pullup on FDpin

Jump to solution
761 Views
jesperselander
Contributor II

pastedImage_1.png

According to the specification on NTAG213F, max. Vdd for pullup on FDpin recommended is 3.6V. I am using a battery 3.3-4.2V as supply. Is that a problem?

Regards,

Jesper

0 Kudos
1 Solution
637 Views
jesperselander
Contributor II

Hi Jorge,

Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.

Best regards,

Jesper

View solution in original post

0 Kudos
4 Replies
637 Views
jesperselander
Contributor II

Hi Jorge,

Thanks for your reply.

I assume  you mean keep VDD voltage below 4.6 V - please confirm.

Best regards,

Jesper Selander

0 Kudos
637 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Jesper,

Sorry for the confusion. No, I meant keeping the voltage below 3.6 V, as specified in the datasheet:

FD_pin.png

Regards!

Jorge Gonzalez

0 Kudos
638 Views
jesperselander
Contributor II

Hi Jorge,

Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.

Best regards,

Jesper

0 Kudos
637 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jesper Selander,

Actually the limiting value for voltage on the FD pin is 4.6 V. But as stated in the datasheet the exposure to limiting values for extended periods can affect device reliability, see below:

pastedImage_1.png

So I highly recommend you to keep VDD voltage below the 3.6 V.

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos