VScode configurations path setup question for SPI communication between RFID and BeagleBone board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VScode configurations path setup question for SPI communication between RFID and BeagleBone board

1,366件の閲覧回数
hhh_hy
Contributor II

For SPI communication between RFID RC522 and BeagleBone board, SPI communication initialization, mode setting, maximum transmission rate setting, and data transmission/reception code were written and executed.

This project was based on vscode and pulled the glibc github.

However, at this time, a cannot open source file "libioP.h" error occurred.

Accordingly, the includepath of vscode's c/c++ configurations was modified as follows to refer to the path /home/debian/RFID/libio where libioP.h exists.

 

${workspaceFolder}/**
${workspaceFolder}/RFID/libio/**

 

At this time, the current path is /home/debian.

I added the path like this, but the related error didn't go away.

The problem above is that when I use the code below I get an error that the source file cannot be opened

 

snprintf(ss_gpio_path, sizeof(ss_gpio_path), "/sys/class/gpio/gpio%d/direction", SS_PIN);

 

In addition, if the code below is used, the following includePath error occurs.

 

// initialize SPI communication 
int SpiInit() {
spi_fd = open(SPI_DEVICE, O_RDWR);
if (spi_fd < 0) {
    printf("Failed to open SPI device");
    return -1;
}

 

#include errors detected. Please update your includePath. Squiggles are disabled for this translation unit (/home/debian/sysdeps/unix/sysv/linux/open64.c).

I wrote the hint ${workspaceFolder}/sysdeps/unix/sysv/linux/x86/include provided by vscode, but, the includePath error doesn't go away.

Should I be more specific in adding routes?

can you tell me about this problem?

 

0 件の賞賛
返信
1 返信

1,270件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, my name is Fabian, I've been assigned to support your case.

I appreciate your interest in our products.

Unfortunately, this is a very old product and, not recommended for new designs.

Since there isn't any software available for this Reader from our side I can't provide any recommendation regarding this issue.

If you are interested in using an MFRC631 plus we have an Application Note (AN11802) that provides the required steps for installing the NFC Reader Library in Linux.

I hope this information may be useful.

Best Regards,
Fabian
0 件の賞賛
返信