To whom it may concern, I would like to understand how NFC tags can be protected from being cloned. Much thanks. C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To whom it may concern, I would like to understand how NFC tags can be protected from being cloned. Much thanks. C

847件の閲覧回数
cesarepoccianti
Contributor I

If it is true that what can be read in an NFC tag can also be copied:

We want to create a software which is able to discriminate between the NFC tags created by us and cloned NFC tags (same url but different tag).

How can this discrimination be made?

0 件の賞賛
2 返答(返信)

588件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Cesare,

Applying higher security level can protect NFC tags from being cloned. Please refer to the following for details.

pastedImage_1.png


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

588件の閲覧回数
cesarepoccianti
Contributor I

Dear Kan Li,

Thanks for your explanation and data on secure NFC tagging.

Can you please further explain how "+ Crypto (w/memory)” is implemented?

Can tags be cryptographically secured without the need of providing passwords to users?

Much thanks

Best

Cesare

Cesare Poccianti

cesare@avoncourt.de <mailto:cesare@avoncourt.de>

Avoncourt Partners GmbH

Maximilianstraße 54

D 80538 München

M +49 15 202 4910 84

T +49 89 716 8030 17

Avoncourt Partners GmbH · Sitz der Gesellschaft: München · Registergericht: München · HRB 215380 · Geschäftsführer: Christian Hostmann, Miguel Papic.

Diese Email enthält ggf. streng vertrauliche und oder rechtlich geschützte Informationen. Das unerlaubte Kopieren, die Weitergabe dieser Email und oder eventuell angehängter Dateien sowie die unbefugte Nutzung der enthaltenen Information ist nicht gestattet. Wenn Sie nicht der richtige Adressat sind oder nicht von diesem autorisiert wurden oder diese Email irrtümlich erhalten haben, informieren Sie freundlicherweise den Absender und vernichten Sie unverzüglich diese Email sowie eventuelle Kopien von ihr und oder ihren Anhängen. Vielen Dank für Ihre Hilfe.

This Email may contain confidential and or privileged information. If you are not the addressee or authorized to receive this for the addressee, you must not use, copy, disclose or take any action based on this message or any information herein. If you have received this message in error, please advise the sender immediately by reply e-mail and delete this message and or potential copies of it or its attachments. Thank you for your cooperation.

0 件の賞賛