Hello I'm running the PN7462AU_ex_ phExCT7816 example and in the fuction phRomhalCt_ColdActivateConfig() always have status 0xC093 (0x93 */ PH_ERR_CT_CLASS_CHANGE_INDICATED, /**< Atr having class indicator came.*/).
Can you help me ? I'm not was doind wrong.
thanks in advance
Did you manage to connect to TDA via ioaux / clkaux?
I have the same symptom - phRomhalCt_ColdActivateConfig - returns an error. And this causes the function does not want to go to read ATR.
I am afraid that the SDK authors have not tested the support for phhalCt_SwitchSlot (E_AUXILIARY_SLOT);
Hello benten,
which chip are you using? The PN7362 does not support contacted. If you want to use contacted cards you have to use a PN7462.
Please have a look at the PN7462 family datasheet and its comparison table: PN7462 Family Datasheet
Best regards,
Alexander
Dear nxf51451,
I use PN7462 - with OM27462CDKP development board and TDA development board.
I found problems (and fix it internaly) to connect with tda (IO_EXT and CLOCK_EXT) like this:
Now it looks that works. My sugestion is - that somebody at NXP should check SDK and try use it with TDA.
Best regards,
Kamil
Hi Kan Li I tried to receibed the ATR .
I had clk_aux in the PN7462 . But not in the PN7362 do you know if this chip support auxiliar slot ?
thanks in advance.
PN7362 has clk_aux on Pin 2, please refer to page 6 from the following link for more details.
http://www.nxp.com/docs/en/data-sheet/PN736X.pdf
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Kan Li the main problem is tha all the functions phRomhalCt_ in ROM in the PN7462 don't work in the PN7362.
For example phRomhalCt_ColdActivateConfig. So that the auxiliary slot don't work autmatically in this chip.
thanks in advance
Hello sergioa,
I think there was a misunderstanding. The PN7362 does NOT support contacted. If you want to use contacted cards you have to use a PN7462 or PN7412.
Have a look at the family datasheet: PN7462 Family Datasheet
Best regards,
Alexander
Hello the problem was in present pin .
Now The card is detected but not ATR is received . I had 0x8A error (PH_ERR_CT_TIME_OUT_ATR_10080ETU, /**< ATR char waiting timeout 10080etu error.*/) in the ProcessActivation function.
Can you help me ?
thanks in advance
Hi Sergio,
This Example Supports 7816 profile for S-Costa card for Ct Module, and supports S-Costa card Activation, MF ,EF Creation and Selection also writes and reads binary to selected EF in Scosta card, so please check if your card is a S-Costa card.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------