PN7462 power sequence with PVDD_IN powered externally

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462 power sequence with PVDD_IN powered externally

ソリューションへジャンプ
896件の閲覧回数
johannesdev
Contributor III

Hi!

I would like to supply PVDD_IN and PVDD_M_IN using an external 3V3 regulator. The datasheet states that PVDD_OUT must be connected to GND in this case (sub-diagram 3):

johannesdev_0-1610715524488.png

However, I ask myself if there is any power sequencing to take into account. Although the external 3V3 will always follow the 5V Vbus voltage on my PCB, is there any delay time or sequence from PVDD_IN to 1V8 (DVDD) or from PVDD_IN to Vbus to respect?

Thanks and best regards,
Johannes

 

0 件の賞賛
返信
1 解決策
881件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

should be no problem

PVDD_IN supply voltage is independent from VBUS supply level.

Have a good day.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
882件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

should be no problem

PVDD_IN supply voltage is independent from VBUS supply level.

Have a good day.

 

0 件の賞賛
返信