PN7462: Reading/Writing multiple tags (ICODE SLIX TypeV) sequentially

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462: Reading/Writing multiple tags (ICODE SLIX TypeV) sequentially

1,240件の閲覧回数
mayank_sharma1
Contributor III

Hi ,

 

Currently, example “NfcrdlibEx5_ISO15693” only reads/writes one tag out of four placed under antenna field as shown in setup image below. I used 4 NXP"s ICODE SLIX TypeV tags for test below. I also set device limit constant to 4 as mentioned in step 2 below.

I need help to modify example “NfcrdlibEx5_ISO15693” in such a way that it selects all four tag one by one and reads/writes data from tags.

 

Question: How to select different tags ( ICODE SLIX TypeV) under antenna field and read/write data to it one by one?

 

I followed following steps for test.

 

  1. Setup with 4 ICODE SLIX type V tags place in field.

         123.png

2. “NfcrdlibEx5_ISO15693” is compiled in NON OS mode with following settings

  • #define PHAC_DISCLOOP_TYPEV_DEFAULT_DEVICE_LIMIT        0x04U
  • phacDiscLoop_SetConfig(&sDiscLoop, PHAC_DISCLOOP_CONFIG_TYPEV_DEVICE_LIMIT, 4) .

 

3. “NfcrdlibEx5_ISO15693” Logs 

 

*** ISO 15693 Example ***

Line: 323   Error - (0x4021) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h

 

Ready to detect

 

Type V / ISO 15693 / T5T Detected

 

UID:  5D 17 D2 27 50 01 04 E0

Product: ICODE SLIX

 

Read Data from Block 3

Read Success

The content of Block 3 is: 75 04 10 00

 

--- End of Read Operation ---

 

Write data to Block 3

Write Success

 

--- End of Write Operation ---

 

--- End of Example ---

 

 

Please Remove the Card

ラベル(2)
0 件の賞賛
返信
0 返答(返信)