我用PN7462的I2C读EPSON 的RTC RX-8025SA,没有读到任何数据,程序如下:
phStatus_t status;
uint8_t bBaudRate;
uint32_t pbuffer[32];
bBaudRate = (uint8_t) ((PH_EXHIF_HW_CRYSTAL_CLK / gpkphCfg_EE_HW_I2CM->dwDataRateHz)
- PH_EXHIF_HW_CRYSTAL_CLK_MHZ);
PH_USER_ASSERT(
phhalI2CM_Init(PH_EXHIF_HW_I2CM_TX_FIFO_THRES,PH_EXHIF_HW_I2CM_RX_FIFO_THRES, \
PH_EXHIF_HW_I2CM_TIMEOUT, PH_EXHIF_HW_I2CM_RETRY_CNT) == PH_ERR_SUCCESS);
/* SDA_HOLD field is 0x0, the I2C Master IP will internal take care of hold time. */
//E_I2CM_7BIT_ADDR_MODE=0x00;
PH_USER_ASSERT(phhalI2CM_Config(bBaudRate, 0x09, /*E_I2CM_7BIT_ADDR_MODE */ 0x00) == PH_ERR_SUCCESS);
do{
status = phhalI2CM_QueueRx(0x32,0x0f,pbuffer);
if (status == PH_ERR_SUCCESS)
{
//
}
调用status = phhalI2CM_Receive(0x32,0x0f,pbuffer);会死机。
如何使用PN7462的I2CM???