Dear Ladies and Gentlemen,
I use following system:
-LPCXpresso V8.2.2 [Build 650]
-Eclipse plugin: com.nxp.pn7xxxxx.update-8.0.0-SNAPSHOT-155.zip
-Development board OM27462CDK
I installed and followed the instruction in UM10883.pdf.
We want to use the device without any RTOS system.
According to manual of UM10883 the example PN7462AU_ex_phExMain should run without RTOS.
Therefore following needs to be set in file "APP_NxpBuild.h"
//#define PHFL_HALAPI_WITH_RTOS
#define PHFL_HALAPI_NO_RTOS
Compilation runs fine also debugging. After some loops in while loop of main function,
the program dies in call of "phhalRf_MFC_Disable();" in file "phhalHw_PN7462AU.c".
There is no return of phhalRf_MFC_Disable(), if I press the "pause" button of debugger,
the debugger stops.
Can anyone help me?
What am I doing wrong?
Does anyone have a running example with NO RTOS of PN7462?
Thank you very much and best regards
Stefan Mueller
Dear NXP,
could you please provide any hints?
Or better, could you please provide a working example for PN7462 without RTOS?
Hello Stefan Mueller,
My apologies for overlooking your question.
Please refer to the reply by colleague Li Kan in the next discussion:
If you still have issues please let me know.
Best Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------