Where can I download user_ee.bin (27.0.0 version) for flashing pn7462 EEPROM.
Hi, gokul
You don't need to download it.
if you develope your application with reader libary, you can find it in Reader Lib directery.
For example:
PN7462AUPspPackageFull-v05_12_00\PN7462AU Software\PN7462AU-FW_v05.12.00_Full\PN7462AU\phHal\phCfg\xml\
if you are using cockpit to connect board, it will be in the path of installation of cockpit.
For example:
PN7462AUPspPackageFull-v05_12_00\PN7462AU Documentation
Have a nice day!
TIC weidong sun
Hi, weidong.sun
If have the version 28.0.0 of user_ee.bin in my package. I wanted to test the card detection with 27.0.0 version of user_ee.bin. So i wanted to check whether the older version (27.0.0) of user_ee.bin is available online.