PN7462: Build error of IAR about the NxpNfcRdLib_PN7462_v06.10.00_Pub

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462: Build error of IAR about the NxpNfcRdLib_PN7462_v06.10.00_Pub

684件の閲覧回数
ZBL
Contributor I

Dears,

When I using IAR to make the example of NxpNfcRdLib_PN7462_v06.10.00_Pub, there are 19 errors, all in the file phhalSysSer_IAR.s, as shown in the figure below, and these errors all appear in the BL command: 

ZBL_0-1619590042112.png

Could you please help handle this problem.

0 件の賞賛
返信
2 返答(返信)

680件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I send the information for the question to your email. Please check your email in time.

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

282件の閲覧回数
CheviN
Contributor I

Hello,

is there a way to share this information with the public? I also encountered this problem today. NXP has not made any changes to phhalSysSer_IAR.s since 2015. I'm using IAR Embedded Workbench 9.20.4, and the IAR assembler simply won't get along with the branches contained within this particular file.

I know that I could just use MCUXpresso, but I'd prefer using the IAR IDE.

Any help will be appreciated.

0 件の賞賛
返信