Hello,
I just wanted some verification on how the Presence Check Command works for the PN7150. Is the command a "subscription" to a notification? Will I continue to receive notifications regarding the presence of an activated remote NFC device after submitting the command once? Or would I have to continuously poll by submitting the command until I received the desired notification?
It seems to be the latter from testing but I keep receiving an unknown error as a notification: 0x4F11. The OID of the command is 0x11; but the remaining byte is unfamiliar and it isn't documented anywhere on the user manual.
Thank you
已解决! 转到解答。
Hello,
As you can see from the NXP-NCI library, the presence check is a blocking function, this means that it waits until the card is removed, please see below:
"PRESENCE_CHECK: perform presence check until tag has been removed (function is blocking until card is removed)"
Hope it helps!
BR,
Ivan.
Hello,
As you can see from the NXP-NCI library, the presence check is a blocking function, this means that it waits until the card is removed, please see below:
"PRESENCE_CHECK: perform presence check until tag has been removed (function is blocking until card is removed)"
Hope it helps!
BR,
Ivan.