Hello,
I try to run example for the PN7150 chip. Unfortunately, the program stops in the function HardFault_Handler. I didn't make changes in the example project. I used the instructions from application note: AN11658.
Hardware:
OM5578/PN7150ARD
LPC1114 LPCXpresso board
Software:
LPCXpresso v8.2.2 [Build 650]
NXP-NCI LPCXpresso example (SW3241) - NXP-NCI_LPC11xx_example
What do you think could be wrong ? Maybe something should be changed in the project properties ? I checked the connections between boards and I think that are correct.
Best Regards,
Adrian Pakosinski