PN532 not detect DESfire EV1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN532 not detect DESfire EV1

5,029 Views
frederictoyon
Contributor I

Hi,

We are using PN532 in a project that use Mifare classic.

Now we need to use DESfire EV1 but this card is never detected by InListPassiveTarget command.

Any one can help us ?

Labels (1)
Tags (2)
9 Replies

745 Views
tsamppa
Contributor II

I also have the exact same problem. Did anyone find any solution?

My PN532 can detect Desfire EV3 2k tag (Yale Doorman) but not Fudan FM-1280 that is ISO 14443-4 complaint.

Android NFC Tools report this Fudan card as Tag type: "ISO-14443-4" and "Mifare DESFire EV1 4k" or just "Mifare Desfire".

 

0 Kudos

2,857 Views
moritzschmidt
Contributor I

Same problem here. Did anyone solve this?

0 Kudos

2,857 Views
linsen
Contributor I

What a poor man, I have the same problem too. Does anyone resolve the trouble?

2,857 Views
annu0412
Contributor II

Please try placing card completely on antenna or try to push it over antenna,this works for me.

I don't know why range for desfire is short very strange.

0 Kudos

2,857 Views
olegoleguello
Contributor II

Hi for all!

I have same problem. I can't polling mifare Plus card with pn532. (all other card polling ok) My settings :
Sam configuration: 0x14 (samConfiguration command), 0x01, 0x14,0x01;
SetParametrs: 0x12(setparametrscommand), 0x12 (DID and RATS  are enabled);
inListPassiveTarget : 0x4a (inlistpassivetarget), 0x01, 0x00;

Help me someone!
With best regards Oleg!

2,857 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Frederic Toyon,

There should be no issues detecting MIFARE DESFire cards with the PN532.

Please provide more details:

What is the command frame you are sending to PN532?

Does the PN532 send back the ACK for the InListPassiveTarget command?

Do you receive some error from PN532 or is the card simply not detected?

Regards!

Jorge Gonzalez

0 Kudos

2,857 Views
maximedeschamps
Contributor I

Hello Jorge Gonzalez,

I’ve got the same problem, I can’t read a DESFire EV1 card whereas a classic card works.

I’m sending this command frame :

0x00

0x00

0xFF

0x04

0xFC

0xD4

0x4A

0x01

0x00

0xE1

0x00

 

I received the ACK Frame from the PN532, but after I verify if the PN532 is ready but it is not. So I can’t see the ERROR code in the response.

Thank’s for your help.

0 Kudos

2,857 Views
frederictoyon
Contributor I

Hi 
Same frame with same result.

Thank's for your help.

2,857 Views
linsen
Contributor I

I don't know whether you fix this problem. but I find that, when I using the AMS1117-3V3 to power the PN532 which setting SPI communication mode. The result like you described. Then, I changed the power IC using xc6233. PN532 find the card immediately. so, first you can examine your power.

0 Kudos