PN5190 lifetime vs operating temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5190 lifetime vs operating temperature

140 Views
sygeryc
Contributor I

Can the PN5190 be run continuously at full power? Some readers with PN5190 show us non-standard behavior - errors in communication with the card, unstable DPC regulation. Readers are used on buses. During operation, the field is always on at full power. The temperature on the chip is in the range of 100-120°C. Readers broken in this way are returned to us after about 1 year of operation. Is the PN5190 built for such operation? Or is it necessary to use LPCD? After replacing the PN5190 with a new one, the reader works correctly again. The problem could also be on the PCB. We use blind vias directly on the soldering pads. But there are no signs of bad soldering on the X-ray. Do you have similar experiences and recommendations with this problem?

0 Kudos
1 Reply

111 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to PN5190 datasheet. 120 is above the maximum operational temperature

danielchen_0-1712574397470.png

 

Regards

Daniel

 

0 Kudos