PN5180 modulation index for ISO14443B设置

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 modulation index for ISO14443B设置

1,349件の閲覧回数
shengdang
Contributor I

Hi,all

我最近在使用PN5180过 EMV Contactless L1时发现typeB 波形的调制深度偏小,因此我想通过修改默认的调制深度(Default modulation index for ISO14443B.)来加大调制深度,但是无论修改

#define PHHAL_HW_PN5180_MODINDEX_I14443B  0xCCU   这个的值调制深度都没有变化。我使用CLRC663时就是用这种方法修改的,但是在PN5180上为什么不行呢,是我改错地方了吗?我应该怎么调整typeB modulation index呢?

/** \name Modulation indices
*/
/*@{*/
#define PHHAL_HW_PN5180_MODINDEX_I14443B  0xCCU /**< Default modulation index for ISO14443B. */
#define PHHAL_HW_PN5180_MODINDEX_FELICA  0x17U /**< Default modulation index for Felica. */
#define PHHAL_HW_PN5180_MODINDEX_I15693  0x10U /**< Default modulation index for ISO15693. */
#define PHHAL_HW_PN5180_MODINDEX_EPCUID  0x10U /**< Default modulation index for EPC/UID. */
#define PHHAL_HW_PN5180_MODINDEX_I18000P3M3  0x10U /**< Default modulation index for ISO18000-3 Mode3. */
/*@}*/

タグ(1)
0 件の賞賛
1 返信

879件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

What value you have set? The range is 0x00 -> 0x1F  (where 0x00 = 100% , 0x1F = 0%)

Also, PHHAL_HW_CONFIG_ASK100 need to be PH_OFF.

For your information, this document may help you.

http://www.nxp.com/documents/application_note/AN11742.pdf 

0 件の賞賛