PN5180 BUSY line still LOW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 BUSY line still LOW

788 Views
LiKe
Contributor I

Dear Sir

I test the PN5180 reader IC, I have a question, the PN5180 busy line still to LOW. 

The PN5180 write Timer0_reload register data can not BUSY line change to High.

I read the Timer0_reload register 

SPI_CS=0;

(void)SPI_send(0x04);

(void)SPI_send(TIMER0_RELOAD);

SPI_CS=1;

delay_ms(100);

SPI_CS=0;

result[0]=SPI_send(0x00);

result[1]=SPI_send(0x00);

result[2]=SPI_send(0x00);

result[3]=SPI_send(0x00);

SPI_CS=1;

the result is right.

I trace the BUSY line by Oscilloscope, the BUSY line to LOW level

but I trace the PN5180 DEMO KIT. The BUSY line can from LOW to High.

Where is the problem? 

Labels (1)
0 Kudos
Reply
1 Reply

721 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Li Ke,

Looks like you toggle the CS line during data exchange. Please kindly refer to the following for details.

pastedImage_1.png

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply