PN512 7-bit I2C address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN512 7-bit I2C address

896件の閲覧回数
pyraohms
Contributor III

I have a custom board for the PN512 that uses I2C addressing. I'm havning a hard time understanding a behaviour that im experiencing:

For I2C mode with "three" bit address, the A1 pin should be set HIGH as per datasheet:

i2c stufff.png

A0 (EA) should be set low, as per datasheet:

i2c stufff.png

Then the pins D5, D6 and D7 can be used to set the I2C address:

pastedImage_3.png

NXP sets the upper 4 bytes to 0101b. I am setting the remaining bits to 111b. So the 7-bit address should be 0101111b = 2F. Instead i detect a unstable I2C address on the bus after power up, either 3F or 07...The chip works in this condition anyway (on these addresses). In an attemt to understand this I changed the A0 (EA) pin to HIGH, and the chip registered on the expected address, 2F. I also changed around D4, D4 and D6 and was able to set addressed that was correct.

So it seems that th A0 (EA) pin is "flipped", it should be HIGH for the three bit addressing to work. That is inconsistent with the datasheet?

Thank you

0 件の賞賛
0 返答(返信)