Hi,
We have system Beaglebone black with Kitkat OS running. I like to integrate OM5577 ie PN7120 NFC kit with beaglebone black and integrate with Android kitkat . The application note mention the same.
refer http://www.nxp.com/documents/application_note/AN11646.pdf
Do anyone build such a system?
venkat
Hello venkatesan,
you can port PN7120 to your android system, but you need to pay attention to the version of android, see here:
-- Android patches for support of NCI based NXP NFC Controllers in KitKat (REV 1.0)
It contains the patch adding support for PN7150/PN7120 to the Android Open Source Project, version KitKat 4.4.4.
Best Regards,
Weidong
Thank you for your reply.
we used the beaglebone black linux, it is working fine in polling mode.
wit the same configuration we ported to android lollipop 5.1.0 with release nfc.nci 3.5.0-LOLLIPOP libraries.
getting error in i2c wirite. attached the screenshot of logcat and dmesgs
could not able to figure out issue in which layer,
HAL, libnfc-nci, JNI and Framework.
Hope the linux driver is fine.
help me to resolve the issue
Hello venkat,
Let us discuss the question in one post(PN7120 integration with android ).
Regards,
Weidong