Hello, I am testing PN5180(OM25180FDK) with NFC cockpit 3.7.
NFC cockpit under ICODE ILT only shows 180003m3 which I assume is ISO18000-3 Mode 3,
Unfortunately I have purchased tags with ISO18000-3 Mode 1. Is there a way to read these tags?
Hello,
It should be not supported depends on the Features of PN5180.PN5180 | Full NFC Forum-compliant frontend IC | NXP . Hope it help you.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------