NXPReaderLib - NTAG424DNA LRP Auth - Unsupported but no error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXPReaderLib - NTAG424DNA LRP Auth - Unsupported but no error

548件の閲覧回数
eljeffo
Contributor III

Across multiple versions of the NXP Reader Library up through the recent NFC Reader Library v07.05.00, it appears that only AES Auth is supported, yet calling LRP will not fail parameter validation.

 

In function phalMfNtag42XDna_Sw_Int_AuthenticateEv2, it notes:

    * bAuthOption should be either one(PHAL_MFNTAG42XDNA_AUTHFIRST_NON_LRP) or zero(PHAL_MFNTAG42XDNA_AUTHNONFIRST_NON_LRP).

 

The only check is:

    if (bAuthOption > PHAL_MFNTAG42XDNA_AUTHFIRST_LRP)

Yet there is no implementation for LRP specific authentication (more specifically, there is no handling of LRPFirst vs LRPNonFirst bAuthOption)

    if (bAuthOption == PHAL_MFNTAG42XDNA_AUTHFIRST_NON_LRP)

    {

        bCmdBuff[wCmdLen++] = PHAL_MFNTAG42XDNA_CMD_AUTHENTICATE_EV2_FIRST;

    }

    else

    {

        bCmdBuff[wCmdLen++] = PHAL_MFNTAG42XDNA_CMD_AUTHENTICATE_EV2_NON_FIRST;

    }

 

Suggest either:

1) Completing the LRP Authentication implementation or

2) Throwing an error until LRP Authentication is available

ラベル(1)
0 件の賞賛
1 返信

538件の閲覧回数
AlexanderB
NXP Employee
NXP Employee

Thank you very much for your feedback. We will plan this for the next release cycle. 

 

Greetings, Alex

0 件の賞賛