NT3H2111 without Energy Harvest - caps ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NT3H2111 without Energy Harvest - caps ?

456 次查看
eperera
Contributor I

If I do not plan on using the energy harvested from the the NFC feilds, but want to be notified when a field is present using the FD pin, do I need capacitors on Vout ? The I2C bus will be powered by the host microcontroller.

0 项奖励
1 回复

354 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

    The main purpose of the capacitance of Vout pin is to decouple, which prevents the parasitic oscillation caused by the positive feedback path formed by the power supply.

    Since you want to use FD function, and the Vout pin must have voltage output at this time, my opinion is to add this capacitor.

Have a nice day!

BR,

Weidong

0 项奖励