Hello,
Can I get the dimensions of the NT2H1611G0DA8 part? Supposed to be in an MOA8 package that is allegedly defined here:
https://www.nxp.com/docs/en/package-information/SOT500-4.pdf
except that's incomplete - even says:
"For unspecified dimensions see PLLMC-drawing given in the subpackage code." - what and where is the subpackage code?
Can you please post the package dimensions, in exhaustive detail, of the MOA8 package?
Thanks!
John
fangfang,
I bought some off of Mouser and I need an NDA to get dimensions of the package? Really?
Why can't I get the device package dimensions?
Can you just tell me if the La pad distance from the Lb pad is approx. 6mm?
Thanks,
johnwest
Hello,
This information is in docstore, please access to the following document in docstore.
Package drawing Dr194641 - MOA8 Package Drawing 3312 062 56531 (4.1) If the customer has the NDA.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------