I'm new to this software and microcontroler. LPCXpresso loads with blinky, the extensions were loaded and specified so the MCU is the NHS3100. I have the NHS3100 demo board on the LPC-Link2 and seen this is able to flash the compiled blinky and templogging examples. Where do I go next ?
Hello Stephen,
Thank you for the screenshot. It looks like you have only imported the blinky application. Any NHS31xx application also depends on a board and a chip library - hence the errors - which are not yet present (physically or linked) in your Eclipse/LPCXpresso workspace.
Have a look at the getting started guide under <SDK>/docs/UM_NHS31xx_GettingStarted.pdf, $2.3 SDK:
A more architectural overview is given in the slides at <SDK>/docs/NHS31xxSoftwareOverview.pdf, which will help in understanding the setup of the SW.
Kind regards,
Dries.
Dries,
I made some progress over the weekend and also got some advice direct from NXP. For the benefit of anyone reading this later;
Follow the Getting Started instructions with the NHS3100 kit to install NHS31xx plugin (section 2.2)
The SDK projects can then be imported from the nss subfolder as described in (section 2.3)
The app_demo_dp_blinkey is however not in a state that it can be built. Changing the projects properties in C/C++Build>MCU Settings to NHS3100 is not enough to fix this demo project.
The Getting Started instructions fail to mention this, and so you fail to get started.
To progress;
Quickstart panel>New Project>Select Wizard NHS3xxx LPCOpenC Project
Take the defaults offered by the Wizard, and on the way name the new project e.g. MyBlinkey
Cut and paste the .c code from the demo project’s mainblinkey.c into the new project just created. In this case mainMyBlinkey.c.
Quickstart panel>Build ‘Myblinkey’[Debug]
And this then builds correctly.
To tidy up, Project Explorer and the workspace can now be cleared of all the original demo project examples but be sure to retain the three library folders, the mods folder and of course MyBlinkey.
With all these removed you can now use the Quickstart panel>Build all projects[]
Stephen.
Hi Stephen,
Excellent you found a workaround. I'm very confused with your post though, so I tried it myself with a newly created workspace.
The blinky project is indeed targeting a generic ARM, but that is OK, as toggling a LED is not an NHS3100 specific feature. It likely becomes a problem when using the blinky project for accessing the TSEN HW block, for example. I'll report this back - it definitely makes more sense to target an NHS3100 IC in the MCU settings.
After building the Blinky project, I could just flash it and see the program in action. And also changing the MCU Settings to NHS3100 - and only changing that - worked for me.
Can you post a direct message to me with your failing project/workspace? I'll try to have a look at why things are messed up and see if a future SDK can improve on this. Can you then also post your OS, your IDE version, and SDK version?
Thanks.
Kind regards,
Dries.