NFC cockpit 15693 configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC cockpit 15693 configuration

ソリューションへジャンプ
2,588件の閲覧回数
tttttttcccc
Contributor I

Hi there,

I am trying to use NFC cockpit to set the configuration of NTAG 5 link to enable energy harvesting. Clev6630BM was used as the NFC reader.

I tried to read the configuration memory first by typing C0043D00 in the Tx data without flags and the flag is set 0x10. Below is the error I have got:

C0 = read_config

04 = manufacturer

3D = Block Address

00 = Block number

tttttttcccc_0-1599553973420.png

I am not sure how to set the flag and if the request command is incorrect.

Please advise. Thank you.

0 件の賞賛
返信
1 解決策
2,555件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi,

Hope you are doing well. You don't need to write the 04h byte, the NXP Manufacturer code is added by the tool. And you would need to set the flags as 02h. You can try with 02 C03D00 and it should work.

2020-09-14_11-50-08.png

 

You can check the 4th webinar of the NFC - NTAG® 5 SPOTLIGHTS. And I would recommend the NTAG 5 Cockpit, it is a specialized tool to work with the NTAG 5. (User Guides: NTAG 5 NFC Cockpit, NTAG 5 I2C Cockpit).

Hope this helps.

 

Best Regards,

Ricardo

元の投稿で解決策を見る

4 返答(返信)
2,544件の閲覧回数
alice1
Contributor II

Is your problem solved? I encountered a similar problem, looking for a solution

0 件の賞賛
返信
2,527件の閲覧回数
tttttttcccc
Contributor I

Yes. It works fine without the manufacturer's code. 

0 件の賞賛
返信
2,515件の閲覧回数
alice1
Contributor II

my tag is CODE-SLIX

NFC reader is  CLEV6630B

But I still can’t send data according to the above operation, I don't know where there is a problem

0 件の賞賛
返信
2,556件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi,

Hope you are doing well. You don't need to write the 04h byte, the NXP Manufacturer code is added by the tool. And you would need to set the flags as 02h. You can try with 02 C03D00 and it should work.

2020-09-14_11-50-08.png

 

You can check the 4th webinar of the NFC - NTAG® 5 SPOTLIGHTS. And I would recommend the NTAG 5 Cockpit, it is a specialized tool to work with the NTAG 5. (User Guides: NTAG 5 NFC Cockpit, NTAG 5 I2C Cockpit).

Hope this helps.

 

Best Regards,

Ricardo