NFC cockpit 15693 configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC cockpit 15693 configuration

Jump to solution
2,310 Views
tttttttcccc
Contributor I

Hi there,

I am trying to use NFC cockpit to set the configuration of NTAG 5 link to enable energy harvesting. Clev6630BM was used as the NFC reader.

I tried to read the configuration memory first by typing C0043D00 in the Tx data without flags and the flag is set 0x10. Below is the error I have got:

C0 = read_config

04 = manufacturer

3D = Block Address

00 = Block number

tttttttcccc_0-1599553973420.png

I am not sure how to set the flag and if the request command is incorrect.

Please advise. Thank you.

0 Kudos
Reply
1 Solution
2,277 Views
nxf58474
NXP Employee
NXP Employee

Hi,

Hope you are doing well. You don't need to write the 04h byte, the NXP Manufacturer code is added by the tool. And you would need to set the flags as 02h. You can try with 02 C03D00 and it should work.

2020-09-14_11-50-08.png

 

You can check the 4th webinar of the NFC - NTAG® 5 SPOTLIGHTS. And I would recommend the NTAG 5 Cockpit, it is a specialized tool to work with the NTAG 5. (User Guides: NTAG 5 NFC Cockpit, NTAG 5 I2C Cockpit).

Hope this helps.

 

Best Regards,

Ricardo

View solution in original post

4 Replies
2,266 Views
alice1
Contributor II

Is your problem solved? I encountered a similar problem, looking for a solution

0 Kudos
Reply
2,249 Views
tttttttcccc
Contributor I

Yes. It works fine without the manufacturer's code. 

0 Kudos
Reply
2,237 Views
alice1
Contributor II

my tag is CODE-SLIX

NFC reader is  CLEV6630B

But I still can’t send data according to the above operation, I don't know where there is a problem

0 Kudos
Reply
2,278 Views
nxf58474
NXP Employee
NXP Employee

Hi,

Hope you are doing well. You don't need to write the 04h byte, the NXP Manufacturer code is added by the tool. And you would need to set the flags as 02h. You can try with 02 C03D00 and it should work.

2020-09-14_11-50-08.png

 

You can check the 4th webinar of the NFC - NTAG® 5 SPOTLIGHTS. And I would recommend the NTAG 5 Cockpit, it is a specialized tool to work with the NTAG 5. (User Guides: NTAG 5 NFC Cockpit, NTAG 5 I2C Cockpit).

Hope this helps.

 

Best Regards,

Ricardo