NFC PN532 radio parameters in ISO/IEC 14443 mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC PN532 radio parameters in ISO/IEC 14443 mode

660件の閲覧回数
rcbtactiq
Contributor I

Can NXP please provide the following information for the PN532 device while operating with IEC 14443 compliant NFC tags?

  • ITU emission designator(s)
  • Channel bandwidth
  • Output power
  • Nominal duty cycle of Tx and class
  • Maximum duty cycle of Tx

 

I was unable to find this in the datasheet / user manual

Kind regards

Reuben

ラベル(1)
0 件の賞賛
1 返信

441件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Reuben,

Actually these parameters depends on your application, and controlled by the up layer application code, please kindly refer to Types of radio emissions - Wikipedia  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛