NFC Forum type 4A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Forum type 4A

1,162 Views
andrewbarningha
Contributor III

Please can anyone advise me what devices NXP do which support NFC Forum type 4A with I2C interface.

I have been using the NT3H1101 device but need to use the forum type 4A.

Thanks

2 Replies

1,006 Views
manojrohitvempa
Contributor II

Hello,

You can use NFC-explore which has Pn512 nfc Transponder. The NFC Reader library can be used as the Software which has both SPI and I2C Interface.

The demo explore-nfc Basic uses SPI Interface.

1,006 Views
Kan_Li
NXP TechSupport
NXP TechSupport

I am sorry, but so far we just have NFC Forum type 4A tag without I2C interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------