LCRC663 can not get respond

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCRC663 can not get respond

1,149件の閲覧回数
臣柱宣
Contributor I

our company use lcrc663 as an NFC device to read Mifare1 card。

the mcu is IMX6Q,the driver write by myself can send REQA(0x26) and get ATQA (0x04 0x00)from PICC.

but send anticollision (0x93,0x20) can not get respond from picc.

my driver set register as follows:

[ 35.056201] lcrc663-get addr= 0x00 ,reg =0x00
[ 35.056274] lcrc663-get addr= 0x01 ,reg =0x40
[ 35.056348] lcrc663-get addr= 0x02 ,reg =0xA0
[ 35.056421] lcrc663-get addr= 0x03 ,reg =0x1F
[ 35.056494] lcrc663-get addr= 0x04 ,reg =0x00
[ 35.056567] lcrc663-get addr= 0x05 ,reg =0x00
[ 35.056639] lcrc663-get addr= 0x06 ,reg =0x3C
[ 35.056712] lcrc663-get addr= 0x07 ,reg =0x40
[ 35.056785] lcrc663-get addr= 0x08 ,reg =0x07
[ 35.056858] lcrc663-get addr= 0x09 ,reg =0x7F
[ 35.056932] lcrc663-get addr= 0x0A ,reg =0x00
[ 35.057005] lcrc663-get addr= 0x0B ,reg =0x00
[ 35.057078] lcrc663-get addr= 0x0C ,reg =0x80
[ 35.057152] lcrc663-get addr= 0x0D ,reg =0x00

other rigister value is set as 106k 14443A by loadreg and loadprotocol cmd.

the only diffrence between send REQA and Anticollision is 

TxDataNum  (address 2Eh this register change from 0x0f to0x08

Can you help me to find where is the problem? thankyou

0 件の賞賛
返信
3 返答(返信)

996件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Looks like you duplicated the same topic in the thread of LCRC663 只能获得ATQA .


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

996件の閲覧回数
臣柱宣
Contributor I

搞定了,谢谢,请问lcrc663能否调整发射功率大小,比如都是在14443A协议106k频率的情况下调整发射功率?

0 件の賞賛
返信

996件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

data sheet上说“A higher supply voltage at TVDD will result in a higher field strength.”所以你可以调整TVDD来实现,TVDD最大为5.5V,请注意ITVDD的最大值为250mA。

pastedImage_1.png

pastedImage_2.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信