Is that normal practice to put card on top of reader during EMC testing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is that normal practice to put card on top of reader during EMC testing?

Jump to solution
930 Views
ALEX4108
Contributor I

Hi,

I got some troubles when I put a Mifare card on top of contactless reader during EMC measurement. The 5th harmonics at 67.8MHz would be seen and  over the upper limit.

Without the card, the harmonics would be much lower. Even I put a metal plate or wire-ring on top of reader, I didn't see the 5th harmonics.

I just wonder if the harmonics was generated from the card and coupled to the reader to form common-mode noise.

Is it necessary to put the card on top of reader during EMC testing? If yes, any suggestion to suppress the harmonics? 

Thanks and regards,

Alex Poon

0 Kudos
1 Solution
908 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ALEX4108 ,

 

Actually it depends on the certificate you want to have, and normally a card/PICC reference is needed at some position to the reader. We provide a training video regarding EMC design for antenna design, please kindly refer to https://www.nxp.com/video/nfc-antenna-design-6-emc-related-design:ANTENNA-EMC-DESIGN-VIDEO for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
909 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ALEX4108 ,

 

Actually it depends on the certificate you want to have, and normally a card/PICC reference is needed at some position to the reader. We provide a training video regarding EMC design for antenna design, please kindly refer to https://www.nxp.com/video/nfc-antenna-design-6-emc-related-design:ANTENNA-EMC-DESIGN-VIDEO for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos