How to use RFID Discover lite for CLRC663 communication through UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use RFID Discover lite for CLRC663 communication through UART

1,470 Views
martinpeevski
Contributor I

   Hello, I am facing problems to use RFID Discover lite tool for establishing communication with CLRCL663 IC on CLEV663B Blueboard 3.0. When I try to communicate with the chip, on the PC screen is displayed status message for error. You can see it in the attached file.

   Can you help me read an ISO15693 tag with CLRC663 and understand the commands for that? I suppose that RFID Discover will do that for me?


   Thank you in advance!

   Martin Peevski

Labels (1)
0 Kudos
2 Replies

937 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello martin,

   Please refer to the link to use PC RS232 to communicate with RC663 EVK board!

Contactless reader evaluation board|NXP 

Regards,

weidong

0 Kudos

937 Views
martinpeevski
Contributor I

Thank you, Wigros,

I already found in internet the PC RS232

serial after two days of searching. Also try it and done the ISO15693

inventory.

And what about the RFIDDiscover, why it not works for me?

On Thu, 16 Feb 2017 02:27:35 -0700, Wigros Sun wrote:

YOU HAVE

BEEN MENTIONED

by Wigros Sun _in Re: How to use RFID Discover

lite for CLRC663 communication through UART in NXP Community_ - View

Wigros Sun's reference to you

0 Kudos