Hi how secure is the NFC tags made upon MIFARE Classic 1k? Is it protected against data copying and cloning? If so what should be done for this protection? If not, which is the type card we can use to achieve this?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi how secure is the NFC tags made upon MIFARE Classic 1k? Is it protected against data copying and cloning? If so what should be done for this protection? If not, which is the type card we can use to achieve this?

1,204 Views
kpki
Contributor I

Hi how secure is the NFC tags made upon MIFARE Classic 1k? Is it protected against data copying and cloning? If so what should be done for this protection? If not, which is the type card we can use to achieve this?

We have planned to use libnfc to communicate with the tag.

0 Kudos
Reply
1 Reply

929 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Kiran KP:

Thank you for using our NFC community.

MIFARE Classic EV1 offers security with 2 CRYPTO1 keys (48-bit each) per memory sector.

However if your application is security sensitive, we actually recommend using one of our newer MIFARE Plus or MIFARE DESFire products, which offer higher security (e.g. AES encryption).

For an overview of the whole MIFARE product range please see the table in the next link, then you can select one according to your application requirements:

http://cache.nxp.com/documents/line_card/MIFARE_ICs_939775017001_v9_HR.pdf

I hope this helps.

Regards!

Jorge Gonzalez

0 Kudos
Reply