Does anyone have experience with NFC front end serial resonans antennas and their performance?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does anyone have experience with NFC front end serial resonans antennas and their performance?

587件の閲覧回数
slavekprzepiors
Contributor II

Trying to get EMVCo level L1 testing and having some problems with load modulation.

Will the serial resonant antenna help with this?

What would be an advantage of using serial versus parallel in NFC environment?

ラベル(1)
2 返答(返信)

455件の閲覧回数
slavekprzepiors
Contributor II

Thanks Kan for your comment.

My question is rather about the basic transmitting antenna configuration as in picture attached:

pastedImage_1.png

I would like to hear about an experience with series (first picture) NFC transmitting antenna connection.

Advantages any of the above configurations in relation to power transfer, coupling influences and load modulation.

Cheers,

Slavek

0 件の賞賛

455件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Slavek,

Antenna can be taken as serial resonant or parallel resonant circuit. Do you mean the matching way? We call symmetric or asymmetric matching, which can be referred to the design guide on the following link: (symmetric matching can have better Rx sensitivity, but it could cause too high field strength @ 0-1cm) http://www.nxp.com/documents/application_note/AN11740.pdf?fasp=1&WT_TYPE=Application%20Notes&WT_VEND...


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------