Dear NXP developers :
I am working on “ app_demo_dp_tlogger”.
HW: nhs3152 demo board; lpc-link2
SW: LPCXpresso(V8.2.0) ,(release redlib(nohost) Og )
When i trying to download to the target with LPCXpresso,I will get error messages as shown below:
Sometimes 02 failed on connect:Ep(01) target marked as not debugable
sometimes 02 failed on connect:Ee(36) could not connect to core
BTW after init() function in the main() , I wrote about 11 bytes to EEPROM at offset 64 .
I had tried to push reset button , and it does not work.
I am anxious to get your reply
There are some more questions:
Q1,If I want to store some datas (less than 20) to eeprom permanently ,where can i write to?
Q2, where does the tags stored ?
Q3.If the chips are damaged ,how can i solve it ?
THANKS
Hello,
It would be helpful to check the get started guide available in the following link: Get Started with the NHS3152THADADK | NXP
For detailed memory read/write information, please refer to section 8.22 until 8.24.2 of the datasheet.
For any related situation with your product, please contact your distributor.
BR,
Ivan.