Clarification on Padding in SDMReadCtr of NTAG 424 DNA Documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clarification on Padding in SDMReadCtr of NTAG 424 DNA Documentation

250 Views
napangelo
Contributor I

Hi,

I have been reviewing the documentation for the NTAG 424 DNA, specifically referring to the example provided on page 12 regarding the decoding of PICCData (https://www.nxp.com/docs/en/application-note/AN12196.pdf).

In the document, an example of decrypted PICCData is given as follows:

  • Decrypted PICCData: c704de5f1eacc0403d0000da5cf60941
  • PICCDataTag: c7
  • UID: 04de5f1eacc040
  • SDMReadCtr: 3d0000

My inquiry pertains to the SDMReadCtr's padding. Specifically, I am trying to understand how to accurately identify where the padding of zeros begins for the SDMReadCtr, as converting from hex to decimal yields various results based on the assumed start of padding (e.g., 3d = 61, 3d0 = 976, etc.).

Could you please provide guidance on how to differentiate the actual counter value from the padding within the SDMReadCtr? For example, in "SDMReadCtr: 3d0000", how can I distinguish between the hex counter value and the padding to accurately interpret the counter's value?

 

Thanks,

Angelo Napolano

0 Kudos
Reply
1 Reply

185 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Angelo Napolano:

 

SDMReadCtr is a 24-bit unsigned integer.  The SDMReadCtr is reset to 000000h when enabling SDM with ChangeFileSettings.  In cryptographic calculations and represented with binary encoding on the external interface, the SDMReadCtr is represented LSB first.
When represented with ASCII encoding on the contactless interface, it is represented
MSB first.

 

Regards

Daniel

0 Kudos
Reply