Can HTRC110 write and/or read T5577 RFID tags?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can HTRC110 write and/or read T5577 RFID tags?

2,039 Views
arendwierks
Contributor I

Hello,

I have a question about the HTRC110. Can it write/read T5577 RFID tags? I'm currently doing a project where I have to design a reader/writer for these tags.

Hope you can help me.

Thanks in advance.

Best regards,

Arend

Labels (1)
Tags (3)
4 Replies

1,307 Views
dulipmadurasing
Contributor I

Hi all,

I'm also designing a reader for NLIS cattle tags (Passive RFID transponder). As it is mentioned above HTRC110 won't be a help. Is there any other reader IC that I can use for my purpose?

Transponder : 

* Compatible with ISO 11785 & 11784 

* In HDX

* 30mm diameter 

* Passive RFID

NLIS-Cattle-300.jpg

0 Kudos

1,307 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Arend Wierks,

The HITAG Reader ICs are optimized and designed to work with HITAG transponder ICs (HITAG|NXP ) compliant with ISO 11784/85 or ISO 14223 standards. Since T5577 is a third party card type then I cannot say if the reader will work with such card. Sorry for the inconvenience.

Regards!

Jorge Gonzalez

0 Kudos

1,307 Views
dunghoangvan
Contributor I

Dear Jorge,

I can't find the antenna design guide for HTRC110 on NXP Website. Can you share it to me?

0 Kudos

1,307 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Application note AN98080 includes the information about antenna design for HTRC110

http://www.nxp.com/documents/application_note/AN98080.pdf 

Regards!
Jorge Gonzalez

0 Kudos