CLRC663 NXP NFC Cockpit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 NXP NFC Cockpit

1,679 Views
alvinwong1109
Contributor I

I am using CLRC663 evaluation board and try to use this board to read the UID of the tag with ISO15693. I loaded the secondary firmware file(nnc.bin) to the NXP NFC Cockpit, but I failed and the software does not work anymore. I tried to install it again but It still does not work. I think that I have loaded the wrong file to the board. What should I do?

Tags (2)
0 Kudos
4 Replies

1,459 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Tsz Tang Wong,

Please flash LPC firmware by refer: Program the firmware to PNEV5180B board
Since you are using CLRC663 evaluation board, the firmware can be found in C:\nxp\NxpNfcCockpit_v4.8.0.0\firmware\Secondary_RC663\BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin
Then CLEV6630B will be able to connect to Cockpit again.

Cockpit read UID ISO15693.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,203 Views
AlanSbor
Contributor II

Good answer!

Realy work.

Thanks a lot!

 

Alexey.

0 Kudos

1,459 Views
alvinwong1109
Contributor I

hi Robin,

After I flash the LPC FW, it comes to another error and it is still disconnected.error2.png

0 Kudos

736 Views
Supreeth
Contributor I

We Have the same issue... Please some once answer

 

Regards

Supreeth

0 Kudos