Hi ,
The older CLRC 632 has a "CoderControl" register at address 0x14 with the option to "SendOnePulse - Bit 7" ,so that switching to next slot can be done. This has helped us to list all the 15693 cards available in the RF Field.
The same anti-collision option is not explicitly stated anywhere in the CLRC 663 plus data sheets.
Will it be possible to detect multiple cards using CLRC 663 plus ?
Thanking you,
Xavier
Hi,
If you see this reply could you please share the register settings you set on the CLRC632 to enable ISO15693 inventory command?
Thanks.
Luke
Hello,
There does not seem to be data available of the CLRC632 available, but, while I check about it, I believe this application note can help you in the anticollision implementation, could you please check it and help me confirm if this helps you?
Regards,
Estephania