CLRC663如何实时检测有没有卡靠近或者离开

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CLRC663如何实时检测有没有卡靠近或者离开

跳至解决方案
1,688 次查看
elvyis
Contributor II

大家好,

   我现在用CLRC663已经可以正常读写TypeA和TypeB类型的护照等卡了,但是目前想实现实时检测卡离开或者靠近的功能,但是该检测功能不影响我正在读或者写卡的连续操作(例如我正在不断的发apdu指令进行一层层选目录,读写文件过程中,能实时侦测到我在操作的卡是否离开,如果离开,我就利用该功能得知卡的离开而进行一些异常处理.),问题的难点是, 我的apdu指令选好目录以后,该检测功能不能影响我选好了该目录,因为我后续apdu指令是在前面的选目录apdu指令成功后才能正常执行的. 请问LDPC是否符合我的这点要求? 另外我不需要考虑低功耗,是否有其他方法可以实现该功能?

谢谢各位大佬先了!!!

标签 (1)
1 解答
1,553 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

LPCD可以检测到是否有卡靠近,但对卡被选中后又拿开的情况没法探测,建议在host controller端设一个timer,应答超时的话就可以判定卡已离开。

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,554 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

LPCD可以检测到是否有卡靠近,但对卡被选中后又拿开的情况没法探测,建议在host controller端设一个timer,应答超时的话就可以判定卡已离开。

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,553 次查看
elvyis
Contributor II

谢谢,你的建议帮助很大!!

0 项奖励
回复