CLEV6630B Reading multiple ICODE-ILT tags

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLEV6630B Reading multiple ICODE-ILT tags

496 Views
mahesh2
Contributor I

How to read Multiple ICODE ILT tags using clEV6630B board ? (CLRC663 plus transponder)

I have tried the  advance discovery loop evaluation example by changing the MAX_DEVICE_LIMIT to 50. But it is able to read only up to 8-10 tags even though 30+ tags in the field.

 

1. What is the maximum possible number of ICODE ILT tags we can inventorize using  CLEV6630B board ? The idea is to read

    50+ tags.

2. If the answer to the maximum possible number to the above question is more than 10, what software changes required in the 

Advancdiscovery loop example to inventorize 50+ tags.

#ICODE ILT

Labels (2)
Tags (1)
0 Kudos
1 Reply

414 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Currently the  NXP NFC Reader Library also implements the Type-V anticollision. If you follow the path of the Discovery Loop you will end up at the anticollision function for Type-V in a file called 'phacDiscLoop_SW_Int_V.c', the method 'phacDiscLoop_Sw_Int_CollisionResolutionV(...)' implements the anticollision.

Regards,

Estephania

0 Kudos