有没有PN7462的Android驱动资料?
你好,小雨,
我们没有发行PN7462的android驱动程序,如果你需要在android下使用NFC,建议你使用PN7150,工程师可以使用android NFC SDK编写应用程序。libnfc-nci, HAL,及其驱动程序,android里面都已经支持,但是请注意一下android版本,在PN7150的文档里有说明。
如果你一定要使用PN7462,你需要自己做移植,下面是个人的一些建议:
---如使用SPI接口和处理器连接
请用spidev.c驱动PN7462,在spidev.c里提供上层接口就可以对寄存器读写了,这样做起来比较简单。
Best Regards,
Weidong
你好,weidong
我们选择PN7462主要是因为PN7462能够管理nfc和SAM卡,如果我们使用PN7150,就只具备nfc的功能。您能不能为我们提供一个方案在使用PN7150的同时,还能够管理SAM卡.
13102370205@163.com
发件人: weidong.sun
发送时间: 2017-05-03 14:35
收件人: 小雨 李
主题: Re: - Re: 寻找PN7462Android驱动资料
NXP Community
Re: 寻找PN7462Android驱动资料
reply from Wigros Sun in NFC - View the full discussion
你好,小雨,
我们没有发行PN7462的android驱动程序,如果你需要在android下使用NFC,建议你使用PN7150,工程师可以使用android NFC SDK编写应用程序。libnfc-nci, HAL,及其驱动程序,android里面都已经支持,但是请注意一下android版本,在PN7150的文档里有说明。
如果你一定要使用PN7462,你需要自己做移植,下面是个人的一些建议:
---如使用SPI接口和处理器连接
请用spidev.c驱动PN7462,在spidev.c里提供上层接口就可以对寄存器读写了,这样做起来比较简单。
Best Regards,
Weidong
Reply to this message by replying to this email, or go to the message on NXP Community
Start a new discussion in NFC by email or at NXP Community
Following Re: 寻找PN7462Android驱动资料 in these streams: Inbox
This email was sent by NXP Community because you are a registered user.
You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences