Need of PMSM(BLDC) FOC codes for KINETICS KV1x series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need of PMSM(BLDC) FOC codes for KINETICS KV1x series

1,922 次查看
vigneshkumarp
Contributor III

Hi, I am using my own board of MKV10Z32VLC7 , which uses FOC algorithm to control the PMSM(BLDC) motor. I just ported the codes from MC56F82726 that is working fine with that algorithm. But after the porting and and changed the motor control libraries according to KINETICS its not working here. Am using RTCESL - CM - 4.3 motor control library.

 

Initially the motor runs fine in open loop but after changing to closed loop control(FOC) it stops its rotation.

 

Is there any specific codes available for KV10 series to make FOC algorithm or any existing working codes are available ?

标签 (1)
0 项奖励
回复
1 回复

1,473 次查看
joseftkadlec
NXP Employee
NXP Employee

Hello,

There is an example FOC code for all standard NXP boards with KV and KE series (MCRSP-PMSM v1.2.0) spinning the standard LINIX motor: http://www.nxp.com/products/software-and-tools/hardware-development-tools/freedom-development-boards.... Have a look there.

BR,

Josef